Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Do 3-phase transformers have an option for a Faraday or Electrostatic shield?
Issue:
Availability of Faraday or Electrostatic shields for 3 phase transformers

Product Line:
LV transformers.

Environment:
Transformers

Cause:
Product features

Resolution:
A Faraday shield/electrostatic shield is a selectable option on most Squared/Schneider Electric Three Phase Transformers, or is already installed on any Transformer with the letters "IS" contained in the catalog number.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings