Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are the main breaker NQ panels available with a 200 ampere, 54 circuit single phase interior?
Issue:
200A MB NQ panel available, 54 circuit ,single phase interior

Product Line:
Panelboards.

Environment:
Products sold in the united States.

Cause:
Product features.

Resolution:
The NQ panelboards do have a 54 circuit option in 225A. However, they are available as factory assembled only. They are not offered as merchandised (off the shelf) at this time.

CTA-ID : 2041175

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings