Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are part numbers for the rear mounting hardware for an MH50WP enclosure?
Issue:
Replacement Parts

Product Line:
Panelboards

Environment:
NQ, NQOD,NF

Cause:
Installation

Resolution:
There are two part numbers. Order catalog number 80116-043-51 for the bag assembly, and 80106-137-01 for the rear mounting rail.


CTA-ID : 2041118

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings