Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is a Mono-flat trim ?
Issue:
Definition of Mono-flat trims for panelboards.

Product Line:
Panelboard

Environment:
Product Features

Resolution:
Mono-flat trims are standard flat cover with concealed hinges and screws, available as flush or surface mount.

On a Hinged trim, the whole trim opens from the left side of the panel and has a hinge on the right side of the mat area. This exposes the entire interior gutter of the box where wiring is found.  The smaller door covering the breakers, is hinged on the right as standard and opens independently from the rest of the hinged trim assembly.
The standard Mono Flat cover has a locked door over the breakers only, not the gutter areas which has the wiring.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings