Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
The customer is looking at XPSMC32Z, does this require any programming?
Yes, it does. Customer must configure the inputs and outputs. Ie, the inputs are configured as e-stops, gate guards, light curtains, etc. The outputs are configured as to which inputs will control them, etc. They will need to order part number XPSMCWIN software to program.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings