Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the cable with straight connector for a sensor with K suffix such as XS1M18MA230K ?<br /><br />
Connector is a 3 pin female AC/DC Micro connector. This is reserved for AC applications and can be identified by the double key and 1/2``-20 thread. On newer Telemecanique sensors, the ``K` designator is changed to ``U20`` which is dimensionally and electrically identical.
XSZCK111Y Yellow PVC 2 meters
XSZCK112Y Yellow PVC 5 meters
XSZCK113Y Yellow PVC 10 meters
XZCP1865L2 Black PUR 2 meters
XZCP1865L5 Black PUR 5 meters
XZCP1865L10 Black PUR 10 meters


CTA-ID : 2044847

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings