Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an MP33125, series M01 branch unit?
Issue:
Current design MP33125 repair parts

Product Line:
US Metering Equipment

Resolution:
Only the parts listed below are considered field replaceable:
  • Parts Kit - MM125KIT (one position, meter socket line side through tenant breaker base)
  • Mounting Channel - 7329652001
  • Customer Cover - MP3125C (includes labels)
  • Circuit Breaker RB Cover - BCV
  • Cover Screws - 4020513002K
  • Blank Meter Socket Cover - MMCBK (top position)
  • Meter Socket Cover - MMC
  • Meter Socket Sealing Ring - 2920910001
  • Pull Box Cover - MP34125PC
  • Line Phase and Neutral Lugs - MMLK250
  • Load Neutral and Service Ground Lug Assembly - 7329819855 (includes 5 lugs and the neutral bus bar)
  • Mounting screws for the Load Neutral/Service Ground Lug Assembly:
    • 2142720163 (mounts the top of the assembly to the main neutral bar)
    • 2149020120 (mounts the assembly to the back of the enclosure just below the main neutral bar connection)
    • 2153217161 (mounts the assembly to the Z shaped bracket attached to the inside back of the enclosure at the bottom of the assembly)
  • Z Shaped Bracket - 7329655401 (for mounting the bottom of the load neutral/service ground lug assembly to the enclosure)
  • Mounting Screws for Z Shaped bracket - (2) 2142217101
  • Equipment Ground Lug Assembly - 7329897052 (includes 3 lugs and mounting bracket)
  • Mounting Screws for Equipment Ground Lug Assembly - (2) 2142217101

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings