Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can you use 2 SDSA1175 on a 208Y120V 3-phase system?
Issue:
Installation of SDSA1175 in a 208Y/120V 3 phase system.

Product Line:
Surge Protective Devices (SPD's)

Resolution:
Two SDSA1175 surge protection devices can be installed to provide suppression for 208Y/120 Vac three-phase four-wire services. See wiring diagram below on how it would be wired up for 208Y/120:
SDSA1175 wiring.PNG

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings