Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an MP55125, Series M01 branch unit?
Issue:
Current design MP55125 repair parts

Product Line:
US Metering Equipment

Resolution:
Only the parts listed below are considered field replaceable:
  • Customer Cover, Left Side - MP5125LC (includes labels)
  • Customer Cover, Right Side - MP5125RC (includes labels)
  • Circuit Breaker RB Cover - BCV
  • Cover Screws - 4020513002K (bag of 10 screws)
  • Blank Meter Socket Cover - MMCBK (top left position)
  • Meter Socket Cover - MMC
  • Meter Socket Sealing Ring - 2920910001
  • Pull Box Cover - MM56125PC
  • Line Phase and Main Neutral Lugs - MMLK250 (kit includes three 2-barrel lugs and mounting hardware)
  • Alternate Lug Kits - Refer to Digest
  • LEFT Meter Sockets Load Neutral and Service Ground Lug Assembly - 7329819857 (includes 4 lugs and main neutral bus bar)
  • RIGHT Meter Sockets Load Neutral and Service Ground Lug Assembly - 7329819862 (includes 5 lugs and main neutral bus bar)
  • Mounting Screws for both Load Neutral/Service Ground Lug Assembly:
    • 2142720241 (mounts the assembly to the main neutral bar of the device)
    • 2149020120 (mounts the assembly to the enclosure just below the main neutral bar connection)
    • 2153217161 (mounts the assembly to the bracket in the enclosure at the bottom of the assembly)
  • Equipment Ground Lug Assembly - 7329897052 (2 required; includes 3 lugs and mounting bracket per assembly)
  • Mounting Screws for Equipment Ground lug assembly - (4) 2142217101
  • Parts Kit - MM125KIT (one position, meter socket line side through tenant breaker base)
  • Mounting Channel - 7329652101

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings