Issue:
What is the part number of the head or operator only for the 3 position and 2 position push pull illuminated operator?
Product Line:
Pushbuttons and Operator Interface
Environment:
30mm, Type K, Type SK
Resolution:
9001KR8 Metal or 9001SKR8 Plastic (Momentary Pull - Maintained Neutral - Momentary Push)
9001KR9 Metal or 9001SKR9 Plastic (Maintained Pull - Maintained Push)
Both use for non or non illuminated operators. These are just the basic operators without the color caps. To use for illuminated, remove the translucent spacer or liner (6512240601) and add a light module.
What is the part number of the head or operator only for the 3 position and 2 position push pull illuminated operator?
Product Line:
Pushbuttons and Operator Interface
Environment:
30mm, Type K, Type SK
Resolution:
9001KR8 Metal or 9001SKR8 Plastic (Momentary Pull - Maintained Neutral - Momentary Push)
9001KR9 Metal or 9001SKR9 Plastic (Maintained Pull - Maintained Push)
Both use for non or non illuminated operators. These are just the basic operators without the color caps. To use for illuminated, remove the translucent spacer or liner (6512240601) and add a light module.
Released for: Schneider Electric USA