Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a CUM400CB, Series M01?
Issue:
Repair parts

Product Line:
Combination Service Entrance Device

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
Only the parts listed below are considered field replaceable.
Meter Cover - 4056250650 (also requires insulator and rivets)
Meter Cover Insulator - 4056138202 and Rivets (2) 2430313190
Meter Cover Mounting Screw - 4020513001K (10 screws, but only 1 is required)
Main Breaker Section Cover - 4056258950
Main Breaker Section Cover Mounting Screws - (3) 2142217101
Utility Pullbox Cover - 4056232801 (handles not included)
Utility Pullbox Cover Handles - (2) 2940101103 and Rivets (8) 2430315290
Utility Pullbox Cover Mounting Screws - (2) 4020513001K and (3) Sealing Screws X1299
Interior Deadfront Trim - 7329420650
Interior Deadfront Trim Mounting Screws - 4020513001K (10 screws, but only 6 are required)
Interior Deadfront Trim Handle - (1) 2940101103 and Rivets (4) 2430315290
Meter Base Assembly - 7329490250
Mounting Channel - 4056142003
Factory Installed Main Breaker - LJL36400U31X (mounting Kit S36967 is also required; lugs on the ON end of the breaker must be removed for connection to the busbars; B phase (center) lug should also be removed from the OFF end of the breaker)
Utility Lug Mounting Hardware - 4056211850
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings