Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the maximum short circuit current Rating (SCCR) for ALL of the Square D combination service entrance devices (CSEDs)?
Issue:
Product design features

Product Line:
Combination Service Entrance Devices

Resolution:
For the maximum SCCR of each CSED, see either the current digest pages, the CAD drawing for each catalog number, or the wiring diagram that comes on each device from the factory.
NOTE: The maximum SCCR of any CSED will depend on the lowest interrupting rated main breaker (service disconnect) installed in the device.

LINK to On-Line digest pages = Current On-line Digest
LINK to On-Line CAD dwgs = On-Line CAD dwgs

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings