Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are current transformer in the 66R-xxx family rated for outdoor use?
Issue:
Doe the 66R-XXX include an outdoor rating?

Product Line:
Instrument transformers

Environment:
Installation/specification

Resolution:
No. Per Instruction Bulletin 39000-300-01A: ``Install the transformer in an appropriate enclosure. These transformers are not intended for outdoor use unless surrounded by an enclosure that provides protection from the weather.``

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings