Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the coil burden for a 9998DA2V02?
Issue:
What is the inrush and sealed VA rating for 9998DA Replacement coils?

Product Line:
Class 8910 Type DPA Replacement Coils

Environment:
Definite Purpose Contactors

Resolution:
The inrush is 109VA and the sealed is 10VA
See attached file for the rest of replacement coils

Schneider Electric USA

Attachment(s)
DPA Replacement coils.pdf [413.98 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings