Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can an EE75T151HCT and other Center Tapped (CT) style Transformers be used where the secondary needs to provide a grounded B phase output?

Issue:
Transformers purchased from SquareD/Schneider Electric do not have any of their primary or secondary terminals grounded as they are shipped from the factory

Product Line:
LV Transformers

Environment:
Applies to Low Voltage Transformers by SquareD/Schneider Electric

Cause:
Configuration of  Transformer terminal wiring is dictated by the type of Electrical System desired

Resolution:
Yes.  If wired to provide a grounded B phase output, the X4 terminal must not be bonded to ground, it should remain unconnected

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings