Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the difference between a plug-in and a non-plug-in type 9007AW limit switch?
The difference is in the construction. The non-plug-in type is shallower in depth with the wiring connected to the contact block by screw terminals. To replace the contact block, remove the wiring. In the plug-in type the depth is deeper with the conduit entry in the back half, along with with screw terminals in a socket. The contact block has stabs that plug into the socket. To replace the contacts, remove the contact block without removing the wiring.


CTA-ID : 2046331

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings