Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are the MP Meter-Pak meter center devices supplied with a 5th jaw factory installed in each meter socket?
Issue:
Product Design Features

Product Line:
MP Meter Pak

Resolution:
The ONLY MP Meter-Pak devices with a factory installed fifth jaw kit are the ​ringless devices, catalog number prefixes MPR, MPH, or MPL. These are supplied with 5 jaw meter sockets as standard.
The MP ring type devices, catalog number prefix MP, are supplied with 4 jaw meter sockets, but a field installable 5th jaw kit, catalog number 5J, can be added if required.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings