Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What current carrying bus material is used within the MP Meter-Pak devices?
Issue:
Product design

Product Line:
MP Meter-Pak

Resolution:
The  MP Meter-Pak devices will have a mixture of both copper and aluminum bus components used within the device. There are no all copper MP Meter-Pak devices available.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings