Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can an EZML ringless device with lever type bypass be converted to an EZMT ring type device with test block bypass in the field?
Issue:
Product Design features

Product Line:
EZM metering equipment

Resolution:
NO, the EZML ringless type with lever bypass CANNOT be field converted to a EZMT ring type with test block bypass. Devices cannot have bypasses added, removed, or changed, and devices cannot be converted from ringless to ring type or vice versa.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings