Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What handle lock-offs are available for the breakers in the old NH1B panel?
Issue:
Selection of circuit breaker handle lock-offs for breakers in an obsolete NH1B panelboard.

Product Line:
Obsolete NH1B panelboards.

Environment:
Obsolete NH1B circuit breaker panelboards sold and supported in the USA.

Cause:
Availability of breaker handle lock-offs for the obsolete NH1B panelboard.

Resolution:
The NH1B panel used the I-line breakers. Refer to the Supplemental and Obsolescence Catalog for the list of handle accessories for the I-line breakers.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings