Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the difference between minimum water level change and maximum level water change for the 9034 Closed Tank Float Switches?
Issue:
On what does it depend the minimum and maximum water level change on 9034 Closed Tank Float Switches

Product Line:
Pressure, Vacuum, and Float Switches

Environment:
Class 9034 Closed tank float switches

Resolution:
The difference between minimum and maximum water level change depends on where the pivot point is set for the float linkage. In the photograph, p 22-11, of Digest 174, The vertical post closest to the float rod attachment is vertical The line drawing to its right shows that same vertical post slanted from
upper right to lower left. These represent the two different locations of the pivot point.

For a very deep tank, choose a float switch for maximum water level change, for a shallow tank, choose a float switch with a minimum water level change.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings