Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the part number for the replacement XCSL DC solenoid connector?
ZCKJ921 is the 90 degree female connector for the electromagnet. This comes standard on the XCSL device. It has screw terminal connections inside
and ring for securing the cable.


CTA-ID : 2045411

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings