Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can an EZM ring type meter socket without bypass be field converted to a ring type with test block bypass?
Issue:
Product Design features

Product Line:
EZM Metering

Resolution:
No. Each EZM catalog number is UL listed and labeled to be configured as built and cannot be modified. Also, the EZM meter socket would not have the appropriate cabinet design to be converted to an EZMT. Per UL, one type of unit cannot be converted into another type.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings