Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the 120/240VAC, 60Hz dual voltage coil for an 8536 or 8502 SB* or SC*, Size 0 and 1?
Issue:
120 / 240 Dual Voltage coil for contactor / Starter Size 0 and 1?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Type S Contactors and Starters

Resolution:
The dual voltage coil is obsolete. Order a 120V coil as 31041-400-42, or a 240V coil as 31041-400-51.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings