Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the part number for a replacement lug that is used on a PBTB304, PBTB504, PBTB306 and PBTB506 plug-in cable tap box?
Issue:
Replacement lug that is used on a PBTB304, PBTB504, PBTB306 and PBTB506 plug-in cable tap box

Product Line:
I-Line busway and accessories

Environment:
Replacement

Cause:
Repair/maintenance

Resolution:
Part number is 40251-116-50 (double lug). The lug accepts a wire range from 1/0 to 600 mcm. One lug required per phase and neutral.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings