Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are the series A and A-L type hubs suitable for use on NEMA 3R rated enclosures with or without the use of gaskets?
Issue:
Design features

Product Line:
Load Centers, Combination Service Entrance devices, Meter sockets

Resolution:
The series A and A-L type hubs are designed for use ONLY on enclosures that are supplied with these types of hub opening patterns and are suitable for use with these hubs ONLY. These specific endwall designs have a raised lip with 4 extruded holes for hub mounting screws and no gasket required.

NOTES
1)
Some devices come from the factory with a gasket already mounted to the enclosure on the hub opening and these gaskets do NOT need to be removed when mounting the A or A-L hubs.
2) Some enclosures have bottom endwalls configured for use with the series A and/or A-L type hubs. These enclosures are also supplied with knockouts for cable entry, provisions for hub mounting screws (4 locations), and do not require the use of a gasket.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings