Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is included in I-Line II busway fitting or straight length such as an AP2530G10ST?
Issue:
Are couplings included for I-Line II busway part number AP2530G10ST?

Product Line:
I-Line busway

Environment:
Installation

Resolution:
Yes. When ordering a section of I-Line II busway, a coupling (joint pack) is factory-affixed to one end. In the case of an elbow, the leg that has the joint pack affixed is considered the bolt leg. The end without the joint pack is considered the slot leg.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings