Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the part number for the replacement cover or door of an MH*WPSS enclosure?
Issue:
Part number for replacement cover or door of MH*WPSS enclosure

Product Line:
PTFDS - FD Enclosure Systems

Environment:
Panelboard enclosures sold and supported in the USA.

Cause:
Can the door on a Nema 4/4X stainless steel panelboard enclosure be replaced?

Resolution:
The covers on stainless steel weatherproof enclosures are not replaceable.
The entire enclosure must be replaced.

CTA-ID : 2048428

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings