Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the catalog number for a plug on Surge Arrestor for NQOD and NQ panelboards?
Issue:
Selection of appropriate plug on surge arrestor for NQOD and NQ panelboards.

Product Line:
PTFDS - FD Enclosure Systems

Environment:
NQOD/NQ panelboards sold and supported in the USA.

Cause:
Selection and application of appropriate plug on surge arrestor for NQOD and NQ panelboards.

Resolution:
Use QO2175SB for 120/240 Vac Single Phase 3 wire NQOD panelboards. Two adjacent branch spaces are required for mounting.
Use two QO2175SB for 208Y/120 Vac Three Phase 4 wire NQOD panelboards only. Do not use on 240/120 Vac Three Phase 4 wire applications.


CTA-ID : 2048042

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings