Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the handle lock-off for an EH or EHB circuit breaker?
Issue:
Part number for the Handle lock off for EH and EHB breakers.

Product Line:
Circuit Breakers

Environment:
EH and EHB Circuit Breaker

Resolution:
The HPAEH was a handle padlock attachment for locking EH or EHB circuit breakers (15-100A) ON or OFF. The HLOEH was a screw clamp handle blocking device for 1, 2, and 3 pole EH or EHB circuit breakers up to 60A.

NOTE:
BOTH OF THESE ARE OBSOLETE WITHOUT REPLACEMENT.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings