Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can a 120 V circuit be fed off of a single leg of a QO(B), 2 pole GFI circuit breaker?
Issue:
Can a 120 V circuit be fed off of a single leg of a QO250GFI?

Product Line:
Miniature Circuit Breakers

Resolution:
Yes, be sure to use the right pole to feed the load so that the test button still works.

Exception: QO(B)260GFI doesn't have a load neutral and can ONLY be used with 240 V or 208 V two-wire loads.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings