Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the difference between limit switches XCKJ167 and XCKJ1167?
XCKJ167 has direct opening contacts but XCKJ1167 does not. The ZCKJ11 contact housing is a plug in unit, while the ZCKJ1 is not. Note that the
ZCKJ11 bodies do not have direct opening contacts.


CTA-ID : 2049601

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings