Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are NQ panels available in NEMA 4X enclosures?

Article available in these languages: Spanish

Issue:
NEMA 4X NQ panel enclosures availability

Product Line:
PTFDS - FD Enclosure Systems

Environment:
Panelboard enclosures sold and supported in the USA.

Cause:
Can the NQ panelboard line be ordered with a NEMA 4/4X enclosures.

Resolution:
Yes. NEMA 4 and 4X rated NQ panelboards are available in either stainless or fiberglass construction.
However, they are available as factory assembled only. Not available as merchandised or off the shelf.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings