Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the replacement for a QMB3620?
Issue:
Legacy Cross Reference on obsoleted QMB3620

Product Line:
QMB

Environment:
QMB panelboards built in 1984 or before.

Resolution:
If the interior was built before 1961, there are no switch replacements.  If the interior was built after 1961 but before 1984, the replacement switch would be a QMB364.  If the switch is going to be installed in a QW panel board or switch board, a plug-on extension kit, part number QMB-320-EX, would also be required.
qmb

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings