Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are knockouts and Hub provisions provided in the MP Meter-Pak Meter Centers for cable and conduit entry(or exit) in the enclosures?
Issue:
Product design features

Product Line:
MP Meter Pak metering

Environment:
Knockouts

Cause:
Application

Resolution:
Knockouts and Hub provisions are provided for cable and conduit entry(or exit) on ALL MP Meter-Pak Meter Center enclosures. The Knockouts/Hubs are located in the enclosure to meet appropriate UL/NEC wire bending space. Keep in mind that the Utility compartments(s) are separated and sealed from the customer(tenant breaker) compartments and the cable entry and exit might be restricted to local Utility and code enforcement.

NOTES:
1) It is NOT recommended for additional holes to be drilled and/or punched in the enclosures, But this is left between the installer and local code authority for final approval
2) All hub provisions on the TOP ENDWALLS of MP Meter-Pak devices will have Closing plates on them from the factory.
3) All the sizes and dimensions for the knockouts and hub provisions can be seen on each catalog number CAD Drawing. SEE CAD DRAWING OF EACH CATALOG NUMBER BEFORE ORDERING DEVICE - CAD DRAWING LINK


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings