Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Video: What is the part number for the side plates covering the busway joints on the 225 amp to 600 amp I-Line busway?
Issue:
What is the part number for the replacement side covers for the busway joint on I-line 225A - 600A busway?

Product Line:
Busway

Environment:
5600 225A - 600A I-Line busway

Resolution:
The joint side plates are called tie channels. The part number for a tie channel is 45202-026-01. Two tie channels are required for each busway joint. See video below:

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings