Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What class of fuse do ALL the 600 A general duty safety switches use?

Issue:

Product Design Features

Product Line:
General Duty Safety Switches

Resolution:
The 600 A general duty safety switches accept Class H or K fuses as standard. Options include Class R fuses (field install Class R fuse kit DRK600) and Class T fuses (ONLY for the D326NT and D326NTR). With Class H or K fuses installed, the switch is UL listed for use on systems with up to 10 kA available fault current. With Class R fuses (and DRK600 fuse kit installed), the switch is UL listed for use on systems with up to 100 kA available fault current. For the switches that accept the Class T fuses, the switch is UL listed for use on systems with up to 100 kA available fault current.

NOTE: DO NOT USE RENEWABLE LINK FUSES IN SQUARE D SAFETY SWITCHES. The use of renewable link fuses may adversely affect user safety, impair reliability, and will void the warranty.

Schneider Electric USA

Explore more
Range:
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings