Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the part number for the neutral bonding strap used on 125A and 250A NF panels?
Issue:
Determine the part number for the neutral bonding strap used on 125A and 250A NF panels.

Product Line:
NF panelboards.

Environment:
Products sold in the United States.

Resolution:
The NFBOND12 is the neutral bonding strap kit to be used when required on 125 A and 250 A NF Panelboards.  This kit includes lugs and required screws.  Please note that UL Service Entrance applications also require a main circuit breaker barrier kit.  Please consult the NF Merchandised Main Circuit Breaker interiors pages in Section 9 of the Digest for additional information.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings