Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are terminals T3, T4, M2, and M3 for on the MDGF module (S48891)?
Issue:
Wiring MDGF Module

Product Line:
Molded Case Circuit Breakers

Resolution:
T3 and T4 are an iron core output to the trip unit for the purpose of powering the trip unit electronics.
M2 and M3 are an analog signal; their output is different for a 3 pole or 6 pole breaker and it communicates the level of GF to the trip unit.
MDFG trip does cause the Ig light to light up on the trip unit.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings