Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Does Schneider Electric offer Sealed Resin Epoxy Encapsulated Transformers larger than 75kVA?

Issue:
Specifications may call for large KVA rated Sealed Resin Epoxy Encapsulated Transformers

Product Line:
LV Transformers

Environment:
Applies to Sealed Resin Epoxy Encapsulated Transformers by SquareD/Schneider Electric

Cause:
Sealed Resin Epoxy Encapsulated Transformers are often needed in applications in which the enclosure is impervious to dust, moisture, etc.

Resolution:
Square D by Schneider Electric can supply Sealed Resin Epoxy Encapsulated Transformers Rated up to 30 KVA Three Phase, and up to 25 KVA Single Phase. Larger Sealed, Resin Epoxy Encapsulated Transformers are not offered

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings