Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are the EZM meter branch units supplied with end closing caps for the main bussing?

Article available in these languages: Spanish

Issue:
Current product design parts

Product Line:
EZM Metering

Resolution:
The end closing caps are provided ONLY with the EZM main devices and EZM transition sections. The EZM meter branch devices, bus extensions, elbows, and corner sections are NOT supplied with end closing caps. The left side end closing cap (part number EZMCAP) extends out by 2" and the right side end closing cap (part number EZMSCAP) extends out by 1".

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings