Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Does the RLTB terminal pad kit include any insulators?
Issue:
Are there insulators provided with the RLTB terminal pad kit for R-frame breakers?

Product line:
Molded case circuit breakers

Resolution:
Insulators are provided only for attachment of the RLTB to the mounting pan or enclosure. The L-shaped mounting brackets that are on the ends of the lug pads are made of an insulating material.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings