Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What type of stainless steel is used for NEMA 4/4X/5 stainless steel safety switches?
Issue:
What type of material is NEMA 4/4X/5 enclosure made of?

Product Line:
Safety Switches

Resolution:
Type 304 stainless steel is used as standard on NEMA 4/4X/5 stainless steel safety switches. Type 316 stainless steel is available, however.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings