Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is 8536SHO2S4 ?
Issue:
Why can`t part number 8536SHO2S4 be found in the Square D Digest?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Type S Contactors and Starters

Resolution:
This was a special class 8536 Type SHO2 series B setup specifically for use in NEMA Size 6 or 7 reduced voltage controllers.

This special 3 pole starter consisted the following:

Supplied without line and load terminal markings
supplied without HP ratings on nameplate
Special arrangement of electrical interlocks for class 8606 controllers
special control wiring per C31105-493

This starter will only be sold as a direct replacement in existing controllers

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings