Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the part number for replacement fuse clips for a Model 5 or Model 6 MCC fusible 60A, 600V feeder bucket?
Issue:
Class R replacement fuse clips availability for a Model 5 or Model 6 MCC fusible 60A, 600V feeder bucket

Product Line:
MCC - Motor control centers

Environment:
Model 5 and Model 6 Fusible Feeder buckets

Cause:
Repair or replacement fuse clips

Resolution:
You will need a quantity or 3 - 153034 ( line side standard fuse clips) and quantity 3 - 40512-451-50 (load side class R fuse clips) are required for a Fusible Feeder bucket. These
are not for use on starter bucket units. Those take different parts and are not compatible. - Shonna

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings