Issue:
Product design features
Product Line:
Homeline load centers
Resolution:
The HOM1224M125RBVP is OBSOLETE AND REPLACED WITH THE HOM1224M125PRBVP. But when it was available, it included (1) HOM1224M125RB with (3) HOM120 and (2) HOM230 branch circuit breakers.
Product design features
Product Line:
Homeline load centers
Resolution:
The HOM1224M125RBVP is OBSOLETE AND REPLACED WITH THE HOM1224M125PRBVP. But when it was available, it included (1) HOM1224M125RB with (3) HOM120 and (2) HOM230 branch circuit breakers.
Released for: Schneider Electric USA