Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is included in HOM3040M200RBVP?
Issue:
Product design features

Product Line:
Homeline load centers

Resolution:
It includes (1) HOM3040M200RB Homeline 200A 30 space / 40 circuit maximum rainproof main breaker load center, (3) HOM120 Homeline 20A single-pole circuit breakers, and (2) HOM230 Homeline 30A double-pole circuit breakers (replaces HOMVPRB1).

Note: This catalog number is Pending Obsolescence and the Replacement is HOM3060M200PRBVP

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings