Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is included with the value pack catalog number HOM3040M200VP?

Issue:
Product design features

Product Line:
Homeline load centers

Environment:
Value pack components

Cause:
Installation

Resolution:

The HOM3040M200VP was an older Value pack that is obsolete see below NOTE.

The HOM3040M200VP included a HOM3040M200TC(30 space 40 circuit, main breaker load center) with a equipment ground bar kit, (3) HOM120 single pole 20Amp and (2) HOM230 two pole 30Amp branch circuit breakers.

NOTE: Once stock is depleted on the HOM3040M200VP, it will be replaced by the HOM3060M200PCVP and the new catalog number includes the following:
(1) HOM3060M200PC (Homeline plug-on neutral, 200Amp, 30space- 60 circuit maximum, indoor, main breaker load center),
(3) HOM120 (Homeline 20 A single-pole branch circuit breaker)
(2) HOM230 (Homeline 30 A, double-pole branch circuit breaker)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings