Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the terminal lug data for the QOM2-MM and QOM2-MVH tenant breakers used in the MP meter centers?
Issue:
MP Tenant breakers

Product Line:
MP Meter Pak Tenant Breakers

Resolution:
The terminal lug data (or wire range) for the QOM2 tenant breakers is (1) #4 AWG - 300 kcmil Al/Cu wire.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings