Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
NQ Nema 3R and Door-in-Door Construction
Issue:
Is door-in-door construction available in the Nema 3R NQ panels?

Product Line:
NQ panelboards sold and supported in the USA.

Environment:
Product feature selection.

Resolution:
Yes. However, these can only be built Factory Assembled with a 250A maximum interior, with a 56 inch box only.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings